Folks,
A quick question regarding the units on the y-axis of figure 8:
Just eyeballing the numbers, if we do a noise integration from say 100-10000 Hz, we should get ~ (9900)^0.5 * ~ 10nV/rthz which is roughly 1uV. The number will end up higher, of course, once you integrate the 100-0 hz flicker noise tail, but not 3 orders of magnitude larger (ie: 1mV).
Should the y-axis be in uV instead of mV?
Also, I noticed that a lot of the figures are quoting resistances in watts vs. Ohms. Are these typos, or am I missing something?
Don