This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI Support Team
A request for recommending parts that can replace the following parts has been received from a customer.
UDA1334ATS // NXP
The specifications required by the customer are as follows.
- Input : Digital
- Output : Analog Stereo
- Operating Voltage : 3.3~5V
- Output level: 2VRMS, Single Ended
- Qualified Automotive Certi.
Thanks.
Regards,
MJ
Hello, We have a family of parts PCM510x with 2VRMS DirectPath , 112/106/100dB Audio Stereo DAC with 32-bit, 384kHz PCM Inter.
Another part that is readily available is PCM512x with more or less the same spec
I will consult with the team and see what else they might recommend. I will let you know by end of the week if there is more to recommend.
Regards,
Arash
After consulting with the team, the above recommendation is okay. Let us know if you have any questions.
Kind regards,
Arash