Other Parts Discussed in Thread: DIX9211
Hi!
A while ago I designed a soundbar distribution board that uses the WM8804, which is an audio transceiver that I set up to convert i2s to SPDIF.
This has worked great, but for some reason, certain soundbars don't like the outputted SPDIF signal, and the sound gets all weird. It's almost like the soundbar tries to convert the signal into a surround sound or something.
However, these soundbars do accept the PCM9211 SPDIF signal, so I'll try to use this.
BTW I've done quite a lot of research, and there is simply no way to make the soundbars accept the WM8804 signal. I've tried various settings in both hardware and software mode, but no luck.
Anyways, since the soundbar distribution system is already sold, I have to design a board that takes the existing SPDI signal as an input, converts it to i2s, and then converts it back to SPDIF again. The PCM/DIX9211 is indeed a transceiver, and by looking at the CodecControl interface, it looks like it might work. I do have a PCM9211EVM board to play around with, but I haven't succeeded yet.
I've externally routed all the i2s outputs to the i2s inputs on the board (signal on connector P7 connected to header W11), and I've desoldered U8 (74LCV244) and connected the input optical signal directly to RXIN2.
I can verify that I have a correctly decoded i2s signal on the i2s outputs, and I also have a valid SPDIF signal on the output. Still, there is no sound, so there is clearly something wrong.
How can I turn the PCM9211 into a SPDIF -> I2S -> SPDIF converter?
Thanks!