Other Parts Discussed in Thread: PCM1754
Hi,
We are using PCM1754-Q1 for audio application.
Circuit Details:
iMX8 (SAI) --> PCM1754-Q1 --> TAS5411 --> Speaker
PCM1754 is configured as follows:
Fs = 24 kHz
BCLK = 768 kHz
SCK = 18.432 MHz
Input Sound Source:
Sample Rate = 24 kHz, Duration = 500 ms, Repeated infinitely
Speaker Output:
We found 2 issues when the sound is playing
1) Speaker output is not exactly same as input
2) Noise observed during play
We have checked the I2S data and it is exactly matched with input.
Could you please support us to resolve the above issues?
Thanks and Regards,
Viswanath