This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5624ADDVEVM: Read A4 not 6C

Part Number: TAS5624ADDVEVM

Hello,

I purchased the TAS5624ADDVEVM evaluation board and connected it as per the user guide. When running the GUI, and clicking the Connect button, the AMP_RESET led extinguishes. When I click the Read button, the response is A4 not 6C. When the board is connected I get an automatic output of ~1.5Vpk-pk on both outputs. I can shut down the outputs by clicking the Shutdown check box on the main page of the GUI or on the PWM page, however I cannot adjust the Modulation Index nor any other settings.

I am planning to use the board in BTL mode. What can I do to get the 6C output and the change the setting to control the output?

Regards,
Mustafa