Part Number: PCM5122
Hello,
Since there is no reset pin on the PCM5122, what is the recommended for the part to get a Manuel reset.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The PCM5122 includes power-on reset "function" as shown in Figure 84 of datasheet. With AVDD greater than approximately 2.8 V, CPVDD greater than approximately 2.8 V, and DVDD greater than approximately 1.5 V, the power-on reset function is enabled. After the initialization period, the PCM5122 is set to its default reset state.
Regards,
Arash
Are there any ways to manually rest after the power rails are fully online and above the thresholds.
Thanks