This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Mapping logical channels on Master side

Hello everybody,

I've got the following two questions about channel mapping:

1. Would it be possible (at future FW releases) to map the logical channels on master side dynamically from the Host Controller?

2. Would it also be possible (at FW 1.2) to change the direction of the physical channels (AD0 to AD2) dynamically from the Host Controller.

Our application highly has the need of this flexibility. We would like to give the user the possibility, to set all 4 channels as Inputs, or all four channels as outputs or anything between. If this would not be possible, we always would have to flash a new FW image, what means we would have to store a big amount of images on an external EEPROM or something else.

Regards,

Oliver