Hi,
I am looking for a Speaker Amplifier with the specifications below.
Architecture : Class-D
- Speaker Channels(output) : 1 channels(Mono),
- Output Power : 5W
Actually our client required support for both 5W and 10W speaker support.
Is there any overhead required while selecting Class D amplifier for speaker ?
I mean if I want to use 5W speaker then do I need to select 5W amplifier or I need to provide 50% overhead and select 7W amplifier ?
As well as can I connect 5W amplifier with 10W speaker ?