This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
(1)The attenuator and PGA gain values of each channel will change independently based whether high or low swing mode is chosen. I suppose that yes, there will be some variation between different lots of ICs. why do you ask this?
(2)where are you finding "device parameters" I cannot find this field in any PCM6xx0 documentation. Where did you find the R1,R2,R3 tolerance as 20%?
Max VCM (maximum common mode voltage) is a DC specification.
Regards,
Arthur
Hi Toshiyuki,
I asked around to the design and systems team and this isn't a specification that was noted. however in general the attenuator and PGA will configure themselves to give the proper signal amplitude for the internal ADC. the gain variation due to process shouldnt need your direct consideration.
the Max VCM is the common mode voltage at the inputs. this is the DC voltage that the input signal is centered around.
for example if the common mode voltage is 7.1V, and the signal is 2Vpp. then the peak voltage seen at the input pins would be 8.1V
Regards,
Arthur