This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424E-Q1: TDM8 format

Part Number: TAS6424E-Q1

Hi team,

I would like to know the definition of SAP register 0x03 bit4 TDM slot size.

Does it mean the bit width of the input audio data? or does it mean the TDM slot size which is determined by the ratio of SCLK and fs?

For example, In my setting, fs=48kHz, SCLK=12.288MHz=256xfs, and input audio data width is 16bit. 

In this case, audio data is 16bit, but the slot size is 256/8ch=32bit. 

Should I set 16bit (1) or 32bit(0) in 0x03[bit4]? 

regards,

  • Tsuji-san,

    TDM slot size is how many bit should be sampled in one slot.

    Does it mean the bit width of the input audio data? or does it mean the TDM slot size which is determined by the ratio of SCLK and fs?

    The slot is always 32bit. The slot size is more like data length. So in the example, just keep default 0 would be fine.

    For example, In my setting, fs=48kHz, SCLK=12.288MHz=256xfs, and input audio data width is 16bit.