This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2700EVM: Large DC offset

Part Number: DRV2700EVM

Hi Team,

We have received this inquiry from our customer,

We have a piezo amplifier eval board DRV2700EVM. We were hoping to be able to use it to provide a large DC offset (~30 V) and a tiny (~10 mV) high frequency (~ 1 kHz) signal to a 10 uF piezo. Should this be possible, or is there a reason that the part can't handle even a very small high frequency component if there is a large DC offset?

Regards,

Danilo