This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3263EVM-U: How to use I2C setups from Application Reference Guide

Part Number: TLV320AIC3263EVM-U


Hello team, 

In the Application Reference Guide for this module there are example I2C setups in the folder called SLAC598, however after downloading it I am not sure of how a config would be used.

In PurePath Tools>I2C Command File, these configs cannot be selected as I tried to navigate to config 7.2 and use it. How are they to be used? Is there another menu where the I2C configs are input?

Thank you very much for your time,

Mateusz

  • Hi,

    These scripts are configured to run with the AIC3263 GUI shown here.

    Once you have the GUI open, you can select the "Command" window under the "View" pull down menu and click open to download this configuration file as shown below and hit "Run" to execute the file.

    If you are using the PurePath Console I2C master then you can copy the I2C commands inside the file to the window. 

    "w" is I2C write, "d" is delay and "#" is comment.