This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OP275 Alternative

Other Parts Discussed in Thread: OPA2172

Can anyone recommend a pin-pin compatible dual op amp to the Analog Devices OP275GSZ.  The must have key specs are:

1. SOIC-8 packge

2. Low noise (5nV/RootHz) or lower.

3. Audio output driver for 1K or higher loads. Stable driving capacity loads at low gains e.g., +1V/V.

4. Relatively low quiescent current draw e.g, 2ma or less per amplifier.

5. Rail-Rail input or close to it.

Thanks!