Hello team.
I would like to know if with PCM9211 is possible to design a system with two SPDIF inputs and two SPDIF outputs, like this:
The SPDIF inputs must be sent to a codec via I2S/TDM and the SPDIF outputs must be received via I2S/TDM as well. The sample rate requirement is 48KHz and all inputs and outputs must working in parallel.
Please, let me know others possibilities if the PCM9211 does not fit that use case.
Thanks in advanced.