Part Number: DRV632
Other Parts Discussed in Thread: TPA6138A2
Hi Team,
Does DRV632 can drive 16ohm load? if it can, what's the minimum output amplitude under the condition of VDD=3.3V,Load=16ohm, THD=1%. Thanks.
Best regards,
Yang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yang,
I would recommend to use TPA6138A2 instead, this is pin to pin compatible and it's rated for lower impedance loads.
If you need a combined operation for high and low impedance, I would suggest to evaluate both devices in order to decide which is better suitable for your application.
Best regards,
-Ivan Salazar
Applications Engineer
Hi Ivan,
Thanks for your reply. Does it mean that we are not sure whether DRV632 can be used for lower impedance load?
Best regards,
Yang
Hi Yang,
DRV632 is not rated for lower impedance loads, so performance may not meet data sheet specs.
So I suggest to evaluate the device for performance considerations.
Best regards,
-Ivan Salazar
Applications Engineer
Hi Yang,
Please consider DRV642 part, there may be an offline discussion about this so just want to make sure to use the correct part number.
Either DRV642 or DRV632 should work for 16 ohm load: https://e2e.ti.com/support/audio-group/audio-internal/f/audio---internal-forum/379202/drv632-as-a-headphone-amp/1335426#1335426
Best regards,
-Ivan Salazar
Applications Engineer
Hi Ivan,
thanks for your confirm. We still want to know what's the minimum output amplitude under the condition of VDD=3.3V,Load=16ohm, THD=1%. Could you check it?
thanks.
Best regards,
Yang
Hi Yang,
I'll try on the EVM and report back the results as soon as possible.
Best regards,
-Ivan Salazar
Applications Engineer
Hi Yang,
Attached are the THD+N vs OutVrms numbers for 16 and 32 ohm loads:

Best regards,
-Ivan Salazar
Applications Engineer