This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCMD3140: Can't stream audio from 4 PDM microphones

Part Number: PCMD3140


Hello, 

I am currently testing the PCMD3140 using the PCMD3140EVM. 

I have 4 external microphones (Invensense T5818) that I am trying to stream audio from. 

I am using the PPC3 (V3.2.1) with the following config (4_MIN_CONFIG).

Using this config file, I am not able to stream audio data from 4 microphones. 

I can stream the audio data for up to two microphones, and these are the ones that the mics allocated in the Left-Slot 0 and Right-Slot 0. For the image attached, Channel 1 and channel 3 works but 2 and 4 doesn't respond. This is not microphone dependent and as long as the microphones are attached to the Left-Slot 0 or Right-slot 0 it will work . 

 4_MIC_CONFIG.zip

I did capture the I2S lines using 4 microphones (CH1 :BCLK, CH2: FSYNC, CH3: SDOUT), and seems like the data bits are properly being sent, I just can't hear the audio. 

Do you have any idea of what is happening here? 

Sincerely ,

Tsugumi