Other Parts Discussed in Thread: PCM2704
Hi experts!
We realize that in BD Mode, the under-voltage protection is set at 7.5V. Since our circuit is powered only by the USB port, we must use the 1SPW mode (UVP = 3.4V).
The problem we have with the 1SPW mode, is that we have only 1 input channel (left or right) at the same time. We don’t need a stereo output in our project, but we need to merge the left and right channels that come from a PCM2704.
On the TPA3138, is there a way to use the BTL input configuration (left + right) and the 1SPW mode at the same time?
If not, what is your recommendation to merge the left and right channels into a single channel, if we use the 1SPW mode? (resistors, op amp, audio transformer, IC, etc)
Thank you,
Cameron