This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M:5805 linux 驱动完善

Part Number: TAS5825M
Other Parts Discussed in Thread: TAS2764, TAS5805, TAS6424, TAS2770, TAS2562, TAS2552, TAS5086

贵司论坛上下载的5805驱动经过修改后初步可用于linux-kernel-5,但驱动

缺少很多功能, 目前内核中已支持的TI TAS系列的芯片驱动如下: tas2552 tas2562 tas2764 tas2770 tas5086 tas571x tas5720 tas5805 tas6424

想知道哪一款跟5805m类似,相对照着完善一下5805的驱动 driver, 谢谢!

  • Hi Daigang

    目前内核中已支持的TI TAS系列的芯片驱动如下: tas2552 tas2562 tas2764 tas2770 tas5086 tas571x tas5720 tas5805 tas6424

        These device you mentioned are all not similar with TAS5805. 

        To use the function in 5805, you need to write the right value into the right register address through I2C. They all can be get from PPC3 software, from dumped file. Check "Include Comments" will help you know the use for most of the codes.