Part Number: TAS5421-Q1
I have designed in the TAS5421 amp to drive a specially wound coil whose DCR is just over 3 ohms. The input to the amp is being fed by a DSP PWM output operating in full symmetry. There are multi-pole filters between the DSP and the amp to give a more sinusoidal input. Gain is set to 20dB. What I am seeing is the IC will often assert the fault pin when the signal is initiated. Per I2C an overcurrent fault is recorded. Other times it operates without issue. A high-frequency current probe on the output shows the max current detected is less than 500mA, nowhere near the 3.5A threshold. Any guidance you can provide would be useful, but 2 specific questions:
1. What does an input over the 1Vrms recommended max result in? Could an input slightly greater cause the fault detection circuits to falsely trigger?
2. The datasheet mentions a "diagnostic cycle" for the fault detection. What triggers this cycle? How long before a fault will clear? If I can remove the failure entirely, that is preferred, but if I know how to deal with it, that will be satisfactory.