Other Parts Discussed in Thread: TAS2505-Q1
Dear all,
In order to design a short to Vbat protection circuit for class D amplifier output, I would need to know after how much time the devices would be damaged if a short to Vbat occurs.
The class D amplifiers I will be working with for these projects are the following ones:
- TAS2552 (24V short to Vbat occuring on the output)
- TAS2505-Q1 (12V or 24V short to Vbat occuring on the output)
If you could give me this information, it would be really helpful
Regards,
Paul-Ambroise Burdet