This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424E-Q1: OUTPUT phase register

Part Number: TAS6424E-Q1


Dear Audio MPA BUs,

This is Koki Tsushima.

Q1

My customer do not understand how register should be for output phase on 0x62.

As highlight in pink on Fig9-16 and Table9-12, this bit should be 2bit.

But as highlight in blue on  Table9-12, this bit should be 3bit.

- I think MSB is for Miscellaneous Control 5 Register, Bit 5 must be set to '1',

   and other lower 2bit xx is for 1-0bit of Miscellaneous Control 2 Register.  Is this correct?

And as process flow we are understanding as follows. - Is this correct?

1. Standby mode and bit5 =1 at 0x28

2.  Setting lower 2bit xx is for 1-0bit of Miscellaneous Control 2 Register

3. Standby enable

We are confusing when we have to STANDBY.

Q2

According to DS, setting of output phase should be done when Standby.

Customer understood that this means that setting of output phase should be done when pin24 is low.

Is this correct?

If this is true, customer wants to set all register setting while Standby=low and then Standby enable.

For that time, is that all register setting can be set correctly?

Cusutmer wants to set all register when standby.

Best 

Koki Tsushima

  • Tsushima-san,

    Q1.  The sequence is correct for setting the output PWM phase.  You can leave standby after this step if you are finished setting up the I2C registers.    

    Q2.  It is good practice to set the register settings while in Standby mode.  Phase settings as well as PBTL settings must be done while in Standby mode.  

    Regards,
    Gregg Scott