I'm having the same issue as in the thread and I do know how to measure it.
"TPA3255: Premature Clipping and limited output power"
I have a 48V 1000W power supply. Both my board and the TPA3255EVM eval module are behaving the same way. I am using PBTL mode with a 2 ohm resistive load. The signal is clipping (and the clip warning coming on) about 36Vpk that is 72 Vpk-pk. This is about 325W, not the 575W or so max power I should get from the 48V supply. Po=Vp^2/2*RL or Vpk-pk^2/8*RL.
So what am I doing wrong?
thx,
Martin