Part Number: SA5534A
Other Parts Discussed in Thread: NE5534A, , NE5534, SA5534
Hello,
I wanted to ask about the difference of the parts SA5534A and NE5534A. The only difference that I found when checking the datasheet was that the SA5534A is specified for a larger temperature range compared to the NE5534A. From page 5 of the datasheet:
"All characteristics are measured under open-loop conditions with zero common-mode input voltage, unless otherwise specified. For NE5534 and NE5534A, full range is 0°C to 70°C. For SA5534 and SA5534A, full range is –40°C to 85°C."
Is this the only difference between these parts or am I missing something?
Thanks in advance,
Stephan