This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5411-Q1: Min and Max leakage current figures/ Fault pin min. low level input voltage

Part Number: TAS5411-Q1


Dear team,

Our customer is working on TAS5411QPWPRQ1 MONP 22 W AMPLIFIER and need the following data : 

  • Min and max of leakage current .
  • Min of Low level input voltage of the fault pin.

Thanks and rgds

  • Jose,

    On the first bullet, I would need to know what pins you need the leakage current.  On the second bullet, the pull up resistor to 3.3Vdc on the fault pin will define the current in the low level state, so this leakage value is not needed.

    Regards,
    Gregg Scott