Part Number: SRC4392
Previously I reported on problems I was having with the DIR on the SRC4392.
Since then we have put the SRC4392 onto our PCB and while most feature seem to be working I am still having trouble with the DIR. Here is my situation :
I am outputting audio over the DIT and then the DIT is connected to the DIR on input 4. The port B I2S bus is configured to input the signal from the DIR output. The single board computer (SBC) is used to generate and capture audio like this :
SBC -> port B -> DIT -> DIR -> port B -> SBC
Unfortunately the DIR doesn't seem to be working. The clocks aren't being locked and there is no audio coming out of the DIR.
I have absolutely no idea what is wrong with this setup. It is the same problem I was having which I reported in the other question to the forum - which also had no solution. I am a little concerned that this chip is on our PCB and we can't get it to work as a DIR.
Here are the current register settings :
01: 3f
02: 00
03: 09
04: 00
05: 29
06: 03
07: 68
08: 00
09: 00
0a: 00
0b: 00
0c: 00
0d: 1b
0e: 17
0f: 22
10: 00
11: 00
12: 00
13: 00
14: 00
15: 00
16: 00
17: 00
18: 00
19: 00
1a: 00
1b: 00
1c: 00
1d: 00
1e: 00
1f: 00
20: 00
21: 00
22: 00
23: 00
24: 00
25: 00
26: 00
27: 00
28: 00
29: 00
2a: 00
2b: 00
2c: 00
2d: 00
2e: 00
2f: 00
30: 00
31: 00
32: 00
33: 00
status regs below
12: 00
13: 00
14: 00
15: 00
16: 00
17: 00
18: 00
19: 00
1a: 00