This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1690-Q1: I2C initialization command timing

Part Number: PCM1690-Q1
Other Parts Discussed in Thread: PCM1690

Hi team,

At initial power on below, what timing can I start to send I2C initialization command to PCM1690?

Is that after 3846 x SCLK clock cycle, or is that OK to send during internal reset mode?

regards,

  • Hi, the data sheet says that initialization is triggered automatically once VDD reaches 2.2V. If you need to make changes after that, for best results you should wait until the power down state is released and the device resumes normal operation. 

    Best regards,

    Jeff