This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: Software and Hardware support

Part Number: TAS5825M

Hi,

I'm using TAS5755MDFD in my design but it's operating temperature is 0 to 125 degree C. I need a Chip which has operating temperature between -40 to 85 degree C. So I have contacted Online Tech Support team and they have suggested me with these two TAS5825MRHBR , TAS5825MRHBT. 

I wanted to know what are all the changes I need to undergo in Hardware and Software if I'm using this part in my design or Software remains the same. Like any register settings need to be changed.

Thanks in advance...

Thanks,

Arun

  • Hi Arun

        For hardware, you can refer to TAS5825 datasheet, and re-draw the schematic and PCB. The peripheral devices will change.

        For software, the DSP structure is totally different, you need to re-do the music tuning. But TAS5825 use PPC3 to control, which is much easier to use. Shouldn't be very big problems.