This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3113D2: Whether there is a minimum reset voltage

Part Number: TPA3113D2

Dear ,

TPA3113D2, Whether there is a minimum reset voltage ? if yes, what is the value ?

  • Hi

    Do you mean SD pin to power down device? if so, you can refer 6.3 part in datasheet.

    Or do you mean OV/UV protection? The OV shutdown threshold is 22V, the UV shutdown threshold is 6.5V.

    Regards,

    Derek

  • Dear ,

    I restart it When I turn off the power within 10 seconds , the speaker will make noise, I  but if I restart  it  after 10 s, it  will be normal. Attached is the schematic diagram, please help to analyze the reason

    it is probabilistic failure,when the noise occurs , I closed IIS but it is still existed , must pull SD low level (mute function),it will be ok 

    8105.TPA3113.pdf

    capture  voltage image P27/P28 (blue as below) is 2V within 10S:

  • Hi 

    What does IIS mean?

    So you mean you only turn off power but you did not pull SD pin to low before power down power?

    Regards,

    Derek