Part Number: INA1650
Can TI confirm the input decoupling capacitors are mandatory on INA165x? I just experienced two consecutive device failing after connecting both inputs GND of the unused channel. +/-9V symmetrical power was used. The device failed in about 25 minuets and overheated. One of the input to common resistance changed from the initial 500K to 200K, the two inputs shows NC.