This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3120: TLV320ADC3120 initial stereo in differential mode

Part Number: TLV320ADC3120


Hi Team,

I refer to datasheet Page 105 9.2.1.2.1 Example Device Register Configuration Script for EVM Setup, and adjustments according to my settings

,but TLV320ADC3120 right channel cannot be output from SDOUT,and I2S data has always only had data on the left channel,

The ADC input points level is 2Vrms differential.

Register

Description

Default value

Setting value

Setting description

TLV320ADC3120 initial

0x00

Page config

0x00

 

 

0x01

Software reset

0x00

0x01

Enable reset

0x02

Sleep config

0x00

0x81

AREG turn on and wake up

0x07

ASI config 0

0x30

0x70

ASI from TDM to I2S mode

0x08

ASI config 1

0x00

0x20

ASI data enable

0x74

ASI OUT enable

0x00

0xc0

CH1,2 assign to SDOUT

0x75

Power config

0x00

0x60

ADC and PLL turn on

Setting

0x3c

CH1 config 0

0x00

0x04

MIC in, Differential, AC-couple, input impedance 10K

 

TLV320ADC3120_I2S_20220406.pdf