Hello!
I need your help troubleshooting an op-amp (LMV1015-25) that should have a gain of about 16V/V but instead is attenuating my system. The op-amp is soldered on a small printed circuit board (PCB) and is powered through a bigger PCB (I will be including pictures below). In the small PCB I have two input pads (red) through which I can directly provide a voltage input signal (using probes). The output of the small PCB is obtained through the pads on the bottom layer (blue). The small PCB is powered as is instructed in the datasheet using a resistor, capacitor, and 3V battery. The resistor has a true value of 2.19kOhms and the capacitor a true value of 2.07uF. I have confirmed all connections using a multimeter and confirmed the small PCB is being provided power as well. Instead of a gain - my output through the op amp is actually attenuated (0.04 of the original input signal). The input signal (V peak-to-peak) is below the maximum (28mV) as instructed on the datasheet. Is there anything that I am missing that could be doing this? Thank you!
Datasheet: www.ti.com/.../lmv1015.pdf