Hello Expert,
I have some question.
Our customer wants to control on/off intersection of Speaker and HPOUT signal path.
At this time, whenever Class-D Driver and HPOUT Driver are turned on/off at the intersection, Power Up/Down setting is also performed.
Page 1 / Register 32 / bit 7:7 of the Class-D Driver was changed to "0" intermittently, and speaker output is not work.
However, there is no problem in Page 1 / Register 31 / bit 7:7 of HPOUT Driver.
1. Is there a case where the bit 7:7 = '0' is automatically changed even though the Class-D Driver's Page 1 / Register 32 / bit 7:7 = '1" is set?
2. When our customer wants to control on/off intersection of Speaker and HPOUT signal path, please send the register setting sequence that can be set most simply in text file or excel file.
In my opinion, if I set Power Up of the Class-D Driver and HPOUT Driver at the beginning, and control only with Class-D Driver Mute On/Off and HPOUT Mute On/Off, I think that there may no issue, How about your opinion?
I'm looking forward to receiving your good feedback ASAP.
Best regards,
Michael