Part Number: NE5532
Other Parts Discussed in Thread: OPA210
Hi team,
My customer met a problem using NE5532P, here is the schematic and waveform about the output.

You can see the output has ripple. Do you have any good advice?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

here is the waveform about on the PIN1
Chris,
That's oscillation due to phase lag in the feedback. 390k is a high resistance; so even a small capacitance for input pin and circuit board will create a stability issue. As a test, try soldering a 4pF to 22pF capacitor on top of R225.
To fix without a board change (to add such a cap), try changing feedback resistors from [390k, 100k] to [39k, 10k]
Hi Ron,
Thanks for your suggestion.
I will tell customer and get the feedback.
This is a old device, customer want to use to control PWM. Is there any suitable device for this EE?
Chris,
The circuit is a linear amplifier with a gain near 3.3 ; what is the input signal and desired output signal?
It is not good to leave the other amplifier unconnected.
Hi Ron,
Thanks for your reply, the customer want to use the amplifier to generate a PWM to control the MOSFET of the power. The input is a MCU output 3.3V signal. I have suggested customer to use the OPA210 to generate the Pulse.
Chris,
Other gate drivers here
https://www.ti.com/power-management/gate-drivers/products.html#sort=p1130;asc