Other Parts Discussed in Thread: LM3478
Hello,
I am configuring the TAS5828M and I'm having difficulty getting the hybrid feedback PWM mode configured correctly. I have set up the configuration in PPC3 for PBTL (Base/Pro 1.0 48K) mode. I have enabled the Hybrid Pro block and set it for a voltage min of 5.5V and max of 20V with 384kHz PWM and implemented the circuit described in the tool in my custom hardware. I have also enabled the PVDD/AGL/OTFB block and set GPIO1 as Class H in the advanced SRT window.
I see that the GPIO1 pin is providing a PWM signal and it is able to have an impact on the supply voltage through the filter and feedback network connections, but the signal does not switch at 384 kHz and does not reach the max or min voltages under any conditions.
Does the Base/Pro 1.0/48K mode support Hybrid PWM feedback? Have I misconfigured a register perhaps? Could it be that the issues I am experiencing are due to the (I think) preproduction version of this device? The amplifiers on my board say PTAS5828M on the top.
I have included an excerpt of my schematic showing the amplifier and boost designs, as well as the PPC3 file I have configured, screenshots from a python tool showing the TAS5828M registers while playing music, and a series of scope traces.
Image_1 shows the SPK_L+ signal (AC coupled) in yellow, the Hybrid Feedback PWM pin (GPIO1) in blue, and PVDD in purple under the conditions of playing music ad med-high volume. Image_2 shows the same trace zoomed in to see the PWM frequency. Image_3 shows the same traces playing music with 0 volume, and Image_4 shows the same traces with music paused.
The audio from the amplifier sounds great, my only problem/symptom is that the hybrid PWM signal induces a clicking in the power supply that is especially apparent while playing at low volumes (but goes away when music is paused).
Any ideas what is going wrong for my application? Your assistance is greatly appreciated.
Best regards,
Craig Verrill