Part Number: PCMD3140EVM-PDK
Other Parts Discussed in Thread: TLV320ADC3120, PCMD3140, TLV320ADC3140
Hello,
Currently I am testing 4 PDM microphones using the PCMD3140EVM-PDK.
Using the USB interface, I can only collect single audio file with data from all 4 microphones combined.
Instead, I would like to collect audio data for each individual mics separately from the same instant of time (data needs to be synced), and thus would need to be able to separate the audio data.
First of all, is this something that is feasible with the EVAL board, and if so please advise on the best method to do so.
The EVAL user guide (Section 7.3) mentions that the AC-MB can be controlled with MATLAB audio tool box, but by utilizing this is it possible to obtain audio data from individual mic?
Also, is there a way to access the codec (XMOS chip) directly and modify the code?
Sincerely,
Tsugumi