This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Smart Amp support team
I have PP-SALB2-EVM for the speaker characterization. It is available with TAS2555, TAS2557, and TAS2562. I would like to know if it is available with TAS2780. If YES, can you share any documents to use it, if you have?
Thanks
Tamio
Hi Tamio,
TAS2780 EVM has PP-SALB2-EVM HW connection available, however speaker characterization process flow is not enabled on the SW side in PPC3-TAS2780 plugin.
Usually the speaker char process is completed on integrated processing devices like TAS2555, TAS2557 and TAS2563.
Are you planning to run the protection algorithm on the host processor?
Best regards,
-Ivan Salazar
Applications Engineer