Other Parts Discussed in Thread: TLV320AIC20,
Hi,
In our design, we have a CODEC (TLV320AIC20) HDSO+/- output connected to an audio power amplifier(LM3886) to drive a 4ohms or 8ohm speaker. This audio power amplifier supply is directly connected to an aircraft DC bus supply i.e 18Vdc to 32.2Vdc with ambient operating temperature conditions as -20 deg C to +55 deg C.
- We need a power level of “2W into an 8 Ohm speaker “or “5W into a 4 Ohm speaker” for full operating temperature conditions i.e, -20 deg C to +55 deg C. As per the figure-37 in the datasheet of LM3886, output power graph started from +/- 9V supply and I was not clear on power levels to be taken at +/-9V. This Confusion is because at Some places of datasheet it was mentioned as 18V min supply and Some other places of datasheet it was mentioned as 20V min supply. So requesting you Conform on the guaranteed power levels at 18V operating condition in both extreme ends of temperature.