Hi Team,
We configured the tlv codec [tlv320aic3101] in our dts as per written in the Documentation. We are using the driver code [tlv320aic3x.c]. Our master is the processor, which generates Mclk frequency of 12.28 MHz and Bclk of 1.53MHz
DTS FILE
&qupv3_se3_i2c {
 status = "ok";
 tlv320aic3x_codec: tlv320aic3x@18 {
 compatible = "ti,tlv320aic3x";
 reg = <0x18>;
 gpio-reset = &tlv320aic321xx_rst_gpio;
 DRVDD-supply = <&pm6150_l18>;
 AVDD-supply = <&pm6150_l18>;
 IOVDD-supply = <&pm6150_l10>;
 DVDD-supply = <&pm6150_l10>;
 };
};
With the i2cdetect command, its showing that the driver code is using
/ # i2cdetect -r -y 2
 0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- -- -- -- -- -- -- 
10: -- -- -- -- -- -- -- -- UU -- -- -- -- -- -- -- 
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
70: -- -- -- -- -- -- -- --
but while booting we can see that the driver code is using and it gets inside i2cprobe, init and the codec probe from the logs. But we were unable to see the activity on SCL and SDA lines while probing.
Also with manual i2cset command, its able to write and read the data.
The codec is not registered inside the sound card [inside /proc/asound/cards]
but the codec is being registered inside the :
/ # cat /sys/kernel/debug/asoc/codecs 
btfmslim_slave
tlv320aic3x-codec.2-0018
snd-soc-dummy
Please help us to find the root cause,
Regards,
Abhiram