Hi Experts,
When I test the TLV320ADC5120 EVM found the THD+N between Left and Right channel have big gap. I don't understand why and need your support to fix this issue.
test setup:
Power supply: AVDD=IOVDD=1.8V.
Input setup: Single end( 1N and 2N negative input pin connect to ground), input 500mVrms 1Khz sinewave.
PPC3 setup: Single Ended, Line input, 10KΩ input impedance, Gain=odB, 32bit I2S-slave output.
AP input clock is I2S 256fs fs=48K. Test the THD+N in dB.
test result show as below:
THD+N |
Left ch -88.3dB/Right ch -68.1dB (DRE ON, 2.5K, 0dB Gain,500mV input) |
Left ch -87.8dB/Right ch -72.7dB (DRE ON, 10K, 0dB Gain,500mV input) |
Left ch -87.6dB/Right ch -72.5dB (DRE OFF, 10K, 0dB Gain,500mV input) |
2nd test is Without changing any setup except change the power supply to AVDD=IOVDD=3.3V. the Left and Right channel THD+N seems OK.
AVDD=IOVDD=3.3V |
Left ch -92.3dB/Right ch -91.2dB (DRE ON, 10K, 0dB Gain,500mV input) |
Thanks.
Anderson