Other Parts Discussed in Thread: TAS3251, , SRC4392
Hello,
For a series of active 2-way and 3-way speakers I am evaluating the capabilities of the TAS3251 Smart-Amp on a TAS3251EVM board.
Since I need to be able to manipulate the PEQ settings for fine tuning while the speakers are in operation via I2C, i was wondering if this is possible?
I can't find the registers in the register map in PPC3, is there any way to set these registers directly ?
Besides that I am wondering why the sample rates for the 2-way-speaker configuration (Mono 1.1) can't be set to 96kHz or 192 kHz, the SRC4392 should support that if I understand that right ?
Is there a way to support higher sample rates for a two way speaker design ?
Best regards