Hello,
One customer used PCM3168A and met questions, he combined LRCKAD and LRCKDA to connect LRCK of host, combined BCKAD and BCKDA to connect BCK=12.288Mhz of Host. SPI mode, sample rate LRCK:48K MCLK: 12.88M, BCK:12.288M. Reading 0x51 of PCM3168A is 0x7, but DOUT1 has no data output. If PCM3168A worked I2S+2DIN+2DOUT, DOUT has output and work normally, so could you please help to analyze why DOUT has no output with TDM mode?
In addition, below is the log information:
Best regards
Kailyn