- the type of MCU you use
- the circuit diagram of the setup in terms of connections between CC85XXDK and the MCU
- the code to program both the CC85XXDK and the MCU
- details of how both units are programmed
- how the configurator can be used to assist in the programming
- any other details that may be useful to duplicate the setup
- the connections between the 3 devices
- how to program the CC8520
- how to program the AIC3101
- how to program the MCU (assume same TI type as above)
- Can they all be programmed 'together' without having to connect and disconnect each one to program separately
- provide any examples of program that you have for host controlled configurations
- how to program the 3 devices (if not covered above)
- any other reference programs or designs that relate to this configuration