Other Parts Discussed in Thread: OPA2132
Good afternoon. I need to create an equalizer with non-standard frequencies. That is, these frequencies are not spaced at the same intervals.
I found the app webench.ti.com/.../filter-type. But I couldn't figure out how to use it.
I would be very grateful if you show by example the calculation of such a filter for the middle position and for values of 80 and 16000 Hz. The maximum/minimum input and output frequencies are 20 - 20000 Hz.
Thanks!