This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: TPA3255 or TPA3116D2 at 100 kHz

Part Number: TPA3255
Other Parts Discussed in Thread: TPA3116D2

Hello,

We have successfully used your TI TPA3255 Class-D Power Amplifier using a step-up transformer to increase the voltage and match the high impedance of a piezoelectric underwater acoustic transducer in the 43 kHz range.  We now need a Class-D Power Amplifier, also for a high impedance piezoelectric underwater acoustic transducer, to operate in the 50 kHz to 100 kHz range.


The power level of the TPA3255 is about right.  Can it be made to operate from 50 - 100 kHz ?  Or is there something better ?


We were also looking at your TPA3116D2 with its 1.2-MHz Switching Frequency, thinking that it might be better from 50 - 100 kHz, but it doesn't have the needed power level.  Could two of them be operated in a bridge fashion to double the power ?

What is your best product recommendation that could be used for high power Class-D applications like this up to 100kHz ?

Thanks for your help.