Tas5766 has some problems, please help solve them.
1. Under normal conditions, when EQ is not added, DC15V is used to supply 4 ohm load, and the maximum output of horn end is about 9V, which begins to be distorted.
2. When EQ is added, other conditions are the same, and the maximum 2V output at the horn end will be distorted. It is tested with demo board. There must be a problem. Please help to see how to solve it?