I'm working with a third party that has already completed PCB layout for a mono application. This layout has single-ended input with INL- and INR- grounded through capacitors and INL+ and INR+ connected through capacitors in parallel to the audio source. On the output, OUTL+ and OUTR+ are connected together and also connected to one side of the speaker (parallel). OUT- and OUTR- are both grounded, as is the other side of the speaker. Will this work? Will this potentially damage the TPA2016? I note from an earlier question that it is recommended to connect a speaker directly across one of the outputs without grounded for the mono application.