This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424-Q1: Unused Output Channel Connection

Part Number: TAS6424-Q1


Hello,

The TAS6424-Q1 is being used in a current design, and there is desire to reuse but will only need three speaker outputs. Do we have a recommended connection/termination for the unused output channel?

Thank you!

Best,

Jacques St. Louis

  • Hi Jacquest

        If you can always set the unused channel to Hi-Z state, never set it into PLAY, then the unused terminal can be left float. If you can't guarantee that, you can consider keep the BST cap, and use larger resistor like 1Kohm, connect the output to GND.