Part Number: TAS2563
We are using TAS2563 and we can capture the Echo reference channel. But we are seeing an issue with the Echo reference signal when the amplitude is above a certain threshold. The signal gets choppy with lot of periodic discontinuities.
The noise section contains discontinuities and Good section is clean. In put is a amplitude ramp signal sine tone at 1 KHz




We have set ASI selection to Audio in/out.
It almost looks like the I/V sense signals creep in once the signal is above a threshold.
This is always reproducible and signal is clean if the threshold is below 1/12th peak to peak.