Dear team,
Could you please help answer below questions?
1. If the input is AUX input, which input type should I choose, Microphone input or Line input?
2. If the input is AC-coupled, then our device can't support DC fault diagnostic. If I still enable the diagnostic, is there any bad impact?
3. Could you please help clarify DIAG_CFG0 Register bit0=1? When using AC-coupled input, our device can't support diagnostic, then what is this bit meaning?
4. When using AC-coupled input, how do we do diagnostics?
5. When INT_MASK is configured Mask, IRQ won't be triggered, but LTCH bit will still be set to 1 when error occurs, right?
Thanks & Best Regards,
Sherry