Part Number: DIX4192
Other Parts Discussed in Thread: SRC4392,
I am working on a new design and I would like to be able to use SRC4392 as a substitute for DIX4192 in case of supply chain issues in the future. Seems like hardware wise there are only pins 14 and 15 that are different. They are NC on DIX4192 and MUTE and RDY on the SRC4392. I was hoping not to have to add any extra components, so that it can be a straight swap in production and nothing else on the PCB would have to change. I would like to be able to just ground pin 14, but the DIX4192 datasheet says "No internal signal connection, internally bonded to ESD pad". And it says nothing else.
So my questions are:
1. Is it OK if I straight ground pin14 on DIX4192, which would ground this ESD pad and are there any issues with that?
2. OR alternatively - on the SRC4392, what happens if the MUTE pin (14) is left floating (not tied low or high)?
Thanks
Veselin